Technical FAQs

Ask a Question

What is the speed reference the unit runs at when have the possible combinations of LI2 set for PS2 which is two preset speeds on the ATV28 unit?

      LIy                 Frequency Reference
       0         =          LSP ( low speed )
       1         =          HSP ( high speed )

CTA-ID : 2011904
Was this helpful?
What can we do to improve the information ?