Technical FAQs

Ask a Question

Can a Visi/Vac circuit interrupter have cables in and out of a single section?<br />Can this be front access only?<br />What is the capacitor switching rating of the Visi/Vac

Yes, a Visi/Vac circuit interrupter can have cables in and out of a single section. There must not be anything mounted in the rear cable area that would obstruct the cables.
This arrangement could be made as front access only as possible.
Top access will be required and possible front bottom.
The capacitor switching rating of the Visi/Vac Circuit Interrupter is 2400KVAR.



CTA-ID : 2011570
Was this helpful?
What can we do to improve the information ?