Technical FAQs

Ask a Question

What can cause external fault in an ATV58 with the P1 communications bridge.

This P1 communications universal serial communications cable is not made or supported by SquareD - Schneider Electric.
With the P1 communications, an external fault can be caused by the P1 signal timing out. Switch #8 on the P1 module enables and disables the fault--with the fault disabled, the unit will just stop and you will not know why so need to leave it enabled. Switches 5, 6, and 7 set the timeout period. With all 3 switches on, the timeout period is 1 minute. Can try increasing the timeout period to 1 minute and see if that helps.
For questions contact:
Panel-Tec
2607A Triana Blvd.
Huntsville, AL 35805
www.panel-tec.com
sales@panel-tec.com
1-800-869-2026
Outside the USA: (256) 534-8132
FAX: (256) 534-4769


CTA-ID : 2012119
Was this helpful?
What can we do to improve the information ?