Technical FAQs

Ask a Question

How can I interlock between HVL/cc switch and a downstream drive.? The customer wants to disconnect power at the drive before opening the HVL/cc. Can we keylock the HVL/cc in the closed position? Do we have a keylock available with elec interlock contacts from Schneider (I don`t think we can use Kirk locks on HVL/cc)? What options can we offer the customer?<br /><br />

Transferred to Smyrna MV TAG attn: Don Bedwell

Yes, the HVL/cc switch can be locked in the closed position.

Interlocking to other equipment can be done by ordering the key locks from Schneider Canada for the other equipment. This will allow the keys to coordinate.
Have also heard of riveting the two keys together for existing locks.


Confirmed Smyrna TAG response with Dale Swing via tele on 6-10 (Don never called him back)


CTA-ID : 2011898
Was this helpful?
What can we do to improve the information ?