Technical FAQs

Ask a Question

Can the Powersuite software perform an Autotune on a ATV58 drive?<br />

Yes, it can the by going to the TUN setting.
Powersuite must be connected to the drive when performing autotune.
This is in the Adjustments / Drive Control menu under the Optimization tab.
Set the value to Yes. After a few seconds it should say Done.
If the operation is unsuccessful, a message will come up to indicate that it was unsuccessful.


CTA-ID : 2011895
Was this helpful?
What can we do to improve the information ?