Technical FAQs

Ask a Question

Customer needed the temperature rating on a ZB5 and ZB4 Operator?

Storage is -40 to 158 degrees F (-40 to 70 degrees C)
Operation is -13 to 158 degrees F (-25 to 70 degrees C) unless otherwise stated.

Per the Operator Interface Catalog 9001CT0001


CTA-ID : 2011752
Was this helpful?
What can we do to improve the information ?