Technical FAQs

Ask a Question

If two HVL/cc switches with SEM mechanisms have a mechanical interlock bar between them, will this cause any problem with the transfer scheme?

On ajacent HVL/cc switches the mechanical interlock bar prevents parallel operation. It does not cause any problems with the automatic transfer scheme.

CTA-ID : 2011565
Was this helpful?
What can we do to improve the information ?