Technical FAQs

Ask a Question

What key lock applications are available for HVL/cc?

Issue:
What key lock applications are available for HVL/cc?

Product Line:
Medium voltage switchgear.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Key lock applications available for HVL/cc:
SEM mechansim without ground switch: Up to 2 LO locks
SEM mechanism with ground switch: One LO lock

OTM mechansim without ground switch: Up to 2 LO or LC locks
OTM mechanism with ground switch: One LO or LC lock

Ground Switch: Up to 2 LO or LC locks - 2 locks max.


CTA-ID : 2011563
Was this helpful?
What can we do to improve the information ?