Technical FAQs

Ask a Question

How do you select in the Product Selector fuses above 15kV 200E?

To select in the Product Selector fuses above 15kV 200E:
Change the General Screen Fuse Type to ``Boric Acid`` or ``Boric Acid and Current Limiting`` if using both types in a lineup.
Then in the interrupter screen change the Fuse Manfacturer to S&C up to 400E or Cutler Hammer above 400E.

HVL/cc fuse go up to 15kV 480A


CTA-ID : 2011562
Was this helpful?
What can we do to improve the information ?