Technical FAQs

Ask a Question

Can we provide the VT`s for a Circuit Monitor in HVL/cc without having the HVL/cc swiitch as a disconnect?

Yes, we can provide the VT`s for a Circuit Monitor in HVL/cc without having the HVL/cc swiitch as a disconnect?
This is done as an incoming section with voltage transformers in the Product Selector.
The HVL/cc switch is a connvient method of disconnecting and grounding the voltage transformers. It does of course add additional cost to the project.



CTA-ID : 2011561
Was this helpful?
What can we do to improve the information ?