Technical FAQs

Ask a Question

Does Schneider Electric offer a 0.5"(1/2") B-Hub for load centers or safety switches?

Issue:
Product Design Features

Product Line:
B Type Hubs

Environment:
Hub Size

Cause:
Knowledge

Resolution:
No, the smallest B Type hub available is 0.75"( or 3/4") part number B075.



 
Was this helpful?
What can we do to improve the information ?