Technical FAQs

Ask a Question

Is the disconnect used on the enclosed ATV66 power circuit F a circuit breaker or switch?

The power circuits B, D, F, G, H, I, J use Molded-Case Sitches for Disconnect.

The power circuits C, E, K use Motor Circuit Protectors for Disconnect.

CTA-ID : 2012098
Was this helpful?
What can we do to improve the information ?