Technical FAQs

Ask a Question

What is the part number of the exterior handle for the 9991MW1 and for the Class 2510 Type MB or MC NEMA 4/4X glass polyester enclosure?<br />

It is 9998HWA1.




CTA-ID : 2011881
Was this helpful?
What can we do to improve the information ?