Technical FAQs

Ask a Question

How do I select a N3R 38kV HVL/cc duplex main switches with cables out in the product selector?

At this point in time the designs have not been completed for the arrangement at 38kV. The SEM Mechanism mechanical interlock has not been designed either.

As of 06/05/03, it will be best to order dual mains with each main switch having it`s own set of fuses.

These options are in the Medium Voltage Metal Enclosed Product Selector.


CTA-ID : 2011877
Was this helpful?
What can we do to improve the information ?