Technical FAQs

Ask a Question

Can you have in-line (in main bus) current transformers on the last three feeders of an HVL/cc lineup?

Although there is not a standard assembly for this, it can be done.

Window type CTs can be installed on one set of metalclad bell assemblies in a 14.75`` wide bus transition section. It may require an additional transition section to return to the starting bus location.

Note: This application replaces full voltage bar type CTs which will not fit in the HVL/cc structure.

CTA-ID : 2011088
Was this helpful?
What can we do to improve the information ?