Technical FAQs

Ask a Question

Is the gate driver card in the VZ3IM1300... kit interchangeable with the gate driver card in the VZ3IM1400... kit?

Yes.

All the gate driver cards are the same for the three phases of the size 6 drive with same Design but the gate driver for the DB is different.

Also, all the size 6 old style Design A units that do not have the 7th digit of serial number = 1 use one type part # 52012-634-50 (GD1 - GD6) and can not be interchanged with the

new style Design B & C that does have the 7th digit of serial number = 1 use another type part # 52012-634-52 (GD1 - GD6)


CTA-ID : 2011087
Was this helpful?
What can we do to improve the information ?