Technical FAQs

Ask a Question

How is a duplex switch with two sets of fuses entered in the Product Selector?

To enter a duplex switch with two sets of fuses entered in the Product Selector just pick the duplex switches as standard and TAG IN the extra set of fuses under Special Features. Pricing will come from the fuses sections of the pricing guides.

This is a non-standard configuration and is therefore not offered in the Product Selector.


CTA-ID : 2011076
Was this helpful?
What can we do to improve the information ?