Technical FAQs

Ask a Question

What is the speed regulation of the Altivar 28?

The ATV28`s speed regulation is defined as follows: 30% of the motor`s nominal slip rating for frequencies greater than 10% of base frequency. In other words, if a 60Hz motor has a rated slip of 2%, then the speed regulation is 0.3 x 0.02 = 0.006 or 0.6%, provided the drive`s output frequency is above 6Hz.

CTA-ID : 2011334
Was this helpful?
What can we do to improve the information ?