Technical FAQs

Ask a Question

Can we supply 60 feet of control wire per auxiliary contact on an HVL switch?<br /><br />This is a request from Canada.

We can supply 60 feet of control wire per auxiliary contact on an HVL switch. This is not standard procedure and is preferred not to be done.

This is a Canadian request.

The control wire will run through the transformer and into a terminal block in the low voltage switchgear.

TAG # 93 has been created for this requirement.


CTA-ID : 2011072
Was this helpful?
What can we do to improve the information ?