Technical FAQs

Ask a Question

What is the scaling of the analog outputs for the Altivar 58 GPO card when it is set up for motor currency or motor frequency?

When an analog output is programmed for Motor current full scale is twice (200%) the drive controller rated output current (not motor rated current) for Constant Torque applications.
The drive controller output current rating can not be changed.
When an analog output is programmed for Motor frequency full scale is the maximum frequency setting. (tFr in the drC menu. Normally, it is 72 Hz)
The maximum frequency can be changed.


CTA-ID : 2011071
Was this helpful?
What can we do to improve the information ?