Technical FAQs

Ask a Question

Can a 5/15kV HVL switch be manufactured with a reduced height of 84``? This is the main switch to a Monroe transformer. This switch is also 36`` deep.

The standard indoor 5/15kV HVL switch is 90`` high. Reduced heights can be done, but it is best to sell the 90`` standard.

Monroe mades a Model 3 packaged substation which is 85`` high and 36 deep. In this case the 85`` was too high for overhang.

A TAG number has been logged for this special feature.


CTA-ID : 2011070
Was this helpful?
What can we do to improve the information ?