Technical FAQs

Ask a Question

What is the fuse protection used on 35kv switchgear called?

Issue:
What is the fuse protection used on 35kv switchgear called? 

Product Line:
Switchgear.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Blown fuse tripping is not available with 38lV HVL switchgear, but is available with 38kV HVL/cc switchgear. This fuse tripping system is named FuseLogic by Square D Company.
The fuse range would be 10E to 117A.





CTA-ID : 2011065
Was this helpful?
What can we do to improve the information ?