Technical FAQs

Ask a Question

What are the dimensions and the weight on the ATS46 D75N and D88N soft starters?

The entire width of the unit is a = 9.45 in (240 mm), the entire height of unit is b = 13.40 in (340 mm), the entire depth of the unit is c = 9.61 in (244 mm), and the weight is 23.59 lb (10.70 kg).

The dimensions are the same for ... D75N , D88N


CTA-ID : 2011053
Was this helpful?
What can we do to improve the information ?