Technical FAQs

Ask a Question

What are the charges for Special Production Tests for Canada including Corona, BIL and Heat Rise? These tests are to be conducted on a factory order before it is shipped.<br /><br />These are development tests, not production tests.<br /><br />Montreal Airport Expansion

Charges for Special Production Tests for Canada including Corona, BIL and Heat Rise. These tests are to be conducted on a factory order before it is shipped.
These are development tests, not production tests.

Montreal Airport Expansion

Heat Run will require 6 days of testing. All tests complete in 2 weeks or less. These tests require scheduling the lab and personnell and should be avoided if at all possible.

Corona Test $2500 USD Net by Customer per lineup.

Hest Run Test $3150 USD Net by Customer per lineup.

BIL Test $2500 USD Net by Customer per lineup.










CTA-ID : 2011052
Was this helpful?
What can we do to improve the information ?