Technical FAQs

Ask a Question

Will the 9422 CFA CKA CLA cable mechanisms accept the FCL, KCL, LCL circuit breakers?

No, these circuit breaker operating mechanism are not designed or UL approved for use with these high interrupting circuit breakers.


CTA-ID : 2011290
Was this helpful?
What can we do to improve the information ?