Technical FAQs

Ask a Question

Can a neutral bus be run through an HVL/cc lineup?

Issue:
Can a neutral bus be run through an HVL/cc lineup?

Product Line:
HVL.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
A neurtal bus could be run through an HVL/cc lineup by running it in the rear in rear extensions. This is not required 99% of the time because the neutral is normally terminated on the ground bus. This should be avoided if possible. The same is true for all metal enclosed lineups.


CTA-ID : 2011041
Was this helpful?
What can we do to improve the information ?