Technical FAQs

Ask a Question

Can the operating handle of an HVL switch be moved to the right side of the switch?

No, the operating handle of an HVL switch cannnot be moved to the right side of the switch. There is only one design and the handle is on the left.


CTA-ID : 2011040
Was this helpful?
What can we do to improve the information ?