Technical FAQs

Ask a Question

Phase barriers 29329 for NS breakers are supplied in sets of 6. Why 6 and how do they mount to the breaker?<br /><br />

The phase barriers has 6 pieces to accommodate a 4 pole breaker. There will be left over parts for a 2 or 3 pole breaker. They mount in slots between the pole positions.

CTA-ID : 2011038
Was this helpful?
What can we do to improve the information ?