Technical FAQs

Ask a Question

What is the difference between the ATV11H ... units and the ATV11P units which all have the same rest of the part number and rated the same?

The ATV11H units have heatsinks on the back of them and the type P units have baseplates for mounting on steel or aluminum frames.

CTA-ID : 2011036
Was this helpful?
What can we do to improve the information ?