Technical FAQs

Ask a Question

Are the Square D EHB125NF, EHB125NS and EHB125NRB circuit breaker enclosures obsolete?

Issue:
Old product availability

Product Line:
Circuit Breaker Enclosures

Environment:
Enclosure only

Cause:
Maintenance

Resolution:

Yes, these old enclosures are obsolete and no longer available. Consider using a F or the PowerPact H or J frame circuit breaker, with the appropriate enclosure and neutral assembly for the application.


CTA-ID : 2011019
Was this helpful?
What can we do to improve the information ?