Technical FAQs

Ask a Question

What is the maximum voltage rating of the Wiggy voltage tester.

Issue:
Application

Product Line:
Wiggy Voltage Tester

Cause:
Clarifying maximum voltage

Resolution:
600 volts AC, 250 volts DC maximum.


CTA-ID : 2010590
Was this helpful?
What can we do to improve the information ?