Technical FAQs

Ask a Question

Is a QOM200 replacement main breaker still available?

The QOM200 is obsolete. It could be replaced with a QOM2200VH. Short circuit current rating would be restricted to the marking on the load center.

CTA-ID : 2011015
Was this helpful?
What can we do to improve the information ?