Technical FAQs

Ask a Question

Is the ATV28 HU29N4U rated NEMA 1?

Issue:   Is the ATV28 drive rated NEMA 1?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:   No. It is an open style drive that requires an enclosure.


 
Was this helpful?
What can we do to improve the information ?