Technical FAQs

Ask a Question

Can you get the Ethernet option to work on the Econo-Flex because do not see this as a modification option?

Informed that you can obtain the VW3A58310U option and add it to the unit in the field.

Unfortunately this is not offered as a Miscellaneous option but I do not know why they chose to handle it in this fashion..


CTA-ID : 2011009
Was this helpful?
What can we do to improve the information ?