Technical FAQs

Ask a Question

Is the AO on Econo Flex ATV58 unit standard or is an analog option card required?

The analog output is a standard feature on all the current Econo Flex and ATV58 units?

The earlier units did require the use of an analog output card in order to have this functionality.

Units released at 3Q of 2002 that drive controller at least v5.1 IE32 is when the analog output was added to standard unit.


CTA-ID : 2011005
Was this helpful?
What can we do to improve the information ?