Technical FAQs

Ask a Question

Can the 5kV triple barrel DIN fuses be used for FuseLogic fuse tripping for the HVL/cc switch?

No, the 5kV triple barrel DIN fuses cannot be used for FuseLogic fuse tripping for the HVL/cc switch.

These fuse ratings are now locked out of the Product Selector and are 840A, 960A and 1080A. The let thru current of these fuses may damage the HVL/cc switch.


CTA-ID : 2010999
Was this helpful?
What can we do to improve the information ?