Technical FAQs

Ask a Question

Is an 8963CD22D available with a momentary contact arrangement?

Order with deadman control option which can be linked to the operators seat or other actuating member. The switch linkage option include a push type 8962CD24D or a pull type 8963CD23D

The crane control portion of this business is now owned by E. C. & M. Call 1-800-240-1230 for technical support.

CTA-ID : 2010997
Was this helpful?
What can we do to improve the information ?