Technical FAQs

Ask a Question

What is the ordering modification code for the Elapsed Timer for the enclosed ATV66?

The mod number is T16.
Note: Enclosed ATV66 drives can only be ordered using product selector. The product selector will add the appropriate mod number when the desired feature is selected.

CTA-ID : 2011221
Was this helpful?
What can we do to improve the information ?