Technical FAQs

Ask a Question

Can the individual meter socket, UHTRS213B be used for an underground service feed?

Issue:
Product design features

Product Line:
Individual Meter Sockets

Environment:
Service Feed

Cause:
Application

Resolution:
The UHTRS213B is UL listed for both Overhead and Underground Feed. BUT since individual meter sockets are approved by catalog number by each separate Utility company, one MUST check with each specific Utility company for approval BEFORE Installation

Note: when unit is installed for underground service a closing plate, ACP, is required for installation over the hub opening in the top endwall


 
Was this helpful?
What can we do to improve the information ?