Technical FAQs

Ask a Question

What is the accuracy of the ATS46 LCR motor current display and does the unit use the same calculation to provide overload protection?

Observed from French Technical support site that the LCR display is accurate with possible error between 5 to 10%.
This value also is what is looked at for overload protection determination.

CTA-ID : 2010956
Was this helpful?
What can we do to improve the information ?