Technical FAQs

Ask a Question

What is a 31158-297-50?

It is a control signal converter to allow the AI2 on the Altivar 58 to use 0-10 volt signal.
It converts the 0-10 VDC signal to 4-20 ma.
The kit is for use on ALTIVAR 58 (ATV58) Type H, FLEX58 Chassis, and Class 8839 ECONO-FLEX drive controllers. The 0-10 Vdc converter board assembly comes factory installed in ECONO-FLEX drive controllers if MOD J09 is selected, or it can be field installed using this converter kit.

NOTE: On some Econoflex drawings there is a part number 31164-099-50. That number is not valid. 31158-297-50 should be used.

CTA-ID : 2010441
Was this helpful?
What can we do to improve the information ?