Technical FAQs

Ask a Question

What is the undervoltage trip level for the 8804 Omega Paks?

The undervoltage trip level is at 87.5% of rated input voltage. It automatically resets at 95% of rated input voltage.

It is measured off the MCB where it comes from a transformer and is stepped down to 24vac


CTA-ID : 2010509
Was this helpful?
What can we do to improve the information ?