Technical FAQs

Ask a Question

Now that D-Fax is not used, how can literature be obtained?

The D-Fax numbers are not used.
Go to http://ecatalog.squared.com/techlib/
From here select the product type that the literature is for. Continue to select the best option that suits the equipment that the literature is needed for.
The search tool only works well if the exact wording or literature number is used.
We recommend searching for the literature by selecting the product types instead. That way, all of the available literature can be displayed and the most pertinent or recent revision can be used.


CTA-ID : 2011166
Was this helpful?
What can we do to improve the information ?