Technical FAQs

Ask a Question

Will a LXL breaker ground fault option work at240V single phase?

Yes. Use two poles, or one pole and a neutral CT.


CTA-ID : 2010944
Was this helpful?
What can we do to improve the information ?