Technical FAQs

Ask a Question

What are the dimensions and weight for an ATV11HU29M3U.

The total width of unit a = 4.7 in. (117mm), the total height of unit b = 5.7 in. (142mm) and the total depth of unit c = 6.2 in (156mm).
The weight of the unit is 4.0 lb (1.8 kg)



CTA-ID : 2010938
Was this helpful?
What can we do to improve the information ?