Technical FAQs

Ask a Question

Why does the ATV28 unit not output the proper voltage when trying to test drive unloaded?

Issue:   Why does the ATV28 unit not output the proper voltage when trying to test drive unloaded?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   Outoput voltage
 
Resolution:   
You can not test this drive with no motor connected to the output terminals because it is a current driven device.

Would not expect to see appropriate values corresponding up to rated line voltage at high speed because of design of unit, regardless of what torque type have unit set for in Uft menu.


 
Was this helpful?
What can we do to improve the information ?