Technical FAQs

Ask a Question

XUJK06353R3DP: What does R3DP suffix mean?

R3 is a mini style 3 pin AC or AC/DC receptacle. DP is dark operate PNP. The sensor is normally programmable, but since there are only 3 pins available with option R3, there are not enough terminals for all possible program options.

CTA-ID : 2010479
Was this helpful?
What can we do to improve the information ?