Technical FAQs

Ask a Question

What are the numbers for the different support tubes lengths available for the XVAC indicating banks?

XVAC02 = 4`` metal tube
XVAC03 = 16`` metal tube
XVAC04 = 31.5`` metal tube
XVAC027 = 4`` black anodized metal tube
XVAC037 = 16`` black anodized metal tube
XVAC047 = 31.5`` black anodized metal tube


CTA-ID : 2011388
Was this helpful?
What can we do to improve the information ?