Technical FAQs

Ask a Question

Why can I not pick Main Tie Main for HVL/cc Lineup in the middle with feeders on the ends for future growth in the product selector?

It was determined that with barriers the bus could be run for 5kV and 15kV with some changes made to the 15kV barrier assembly.

These changes should be incorporated into the Product Selector for HVL/cc.

These should be changed soon in the selector.


CTA-ID : 2011380
Was this helpful?
What can we do to improve the information ?