Technical FAQs

Ask a Question

Cables on one HVL/cc were brought into the side and another in from the rear. The electrical inspector is questioning if this meets UL?

It is not a UL issue , but more a codes issue. HVL/cc can be configured for side or rear entry and exit. These are special configurations. As long as the bend radius of the cable is sufficient, the cable configuration should be OK.


CTA-ID : 2011379
Was this helpful?
What can we do to improve the information ?